大家都知道280x是双电源供电的,即外围电路采用的是3.3v电源,而内核采用的是1.8v供电,ti提供的参考设计所使用的芯片TPS67D301这类的芯片价格太高,普通的LDO之类的芯片虽然非常便宜,但是不知道会不会导致280x在上电时出现异常现象。我想看下大家有没有采用过LDO这种芯片来实现280x系列芯片的供电。另外数据手册上提供的上电时序容易实现吗?除了参考设计以外,有没有其他的既便宜又可靠的供电实现办法。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家都知道280x是双电源供电的,即外围电路采用的是3.3v电源,而内核采用的是1.8v供电,ti提供的参考设计所使用的芯片TPS67D301这类的芯片价格太高,普通的LDO之类的芯片虽然非常便宜,但是不知道会不会导致280x在上电时出现异常现象。我想看下大家有没有采用过LDO这种芯片来实现280x系列芯片的供电。另外数据手册上提供的上电时序容易实现吗?除了参考设计以外,有没有其他的既便宜又可靠的供电实现办法。
谢谢
您好!
TI有相当多的电源芯片供您选择。会有相关人员把您的帖子转到电源讨论组,会有电源工程师为您解答。
对于F2808来说,3.3V和1.8V是同时供电,或者1.8V先供电。
没有像F2812那样严格的上电要求,因此会有很多电源芯片供您选择。
谢谢!
你好:
关于280X系列的电源设计可通过TI的WEBENCH软件进行设计。可到TI的主页http://www.ti.com/ 右下角,选择FPGA/UP点uP Architect进入后选择TI的280X系列芯片,按提示进行设计。

谢谢jones,我还是有个问题,如果3.3v先上电会不会导致管脚状态不稳定,或者导致芯片无法正常起动。另外,能否推荐一款芯片。3.3v的输出能力为1A。1.8v能够正常供芯片运行即可。