This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

器件选型推荐

Hi,

  我需要两款嵌入式芯片推荐,需求如下:

1,数字对讲机应用,调制解调算法核心DSP芯片:

(1)单核32bit定点型DSP;

(2)工作频率大于100M;

(3)工作温度-40~85;

(4)内部集成256kB SRAM+64kB DRAM,12kB ROM或更高

(5)3路I2S,两路SPI,1路UART,一个USB或者更多

(6)内核电压1-1.3C

2,主控芯片Arm处理器:

(1) 16bit,主频大于150MHz,大于等于1个内核

(2)内核电压≤3.3V,IO电压≤3.3V

(3)指令缓存≥128kB,数据缓存≥128kB

(4)IO数量≥80

(5)PWM输出口数量≥32

是否有合适的EP芯片可供选择?谢谢