This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: config_update模式相关问题

Part Number: BQ76952

专家您好!

       我们在使用BQ7695203这款芯片中,需要对该芯片的TS1,TS3等管脚更改ADIN模式,按照例子程序配置相应RAM后,发现设备并未配置成功,不知是何原因导致。
       调试过程:
       1、进入config_update模式,检查battery_status值为0x018d.
       2、配置相关RAM
       3、退出config_update模式
       4、检查配置RAM,发现该RAM配置不成功,依然为默认值。

问题:1、进行多次RAM写也无法写入,写之间均加入了延时等待。现在不清楚到底什么情况导致RAM写不进去?是有特殊的操作步骤吗?还是对硬件有相应的配置?因为在看OTP操作时,看到要求BAT管脚电压在10-12V之间,是否写RAM也有类似的要求呢?