This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

开关电源IC问题



开关电源IC ICE2A365的功率是多少?能承受多少A的?

  • 这是英飞凌的IC, 功率在45-65W之间...与你的输入范围有关

    Type Package VDS FOSC RDSon

    1)

    1) typ @ T=25°C

    230VAC ±15%2)

    2) Maximum power rating at Ta=75°C, Tj=125°C and with copper area on PCB = 6cm²

    85-265 VAC2)

    ICE2A0565 PG-DIP-8-6 650V 100kHz 4.7Ω 23W 13W

    ICE2A165 PG-DIP-8-6 650V 100kHz 3.0Ω 31W 18W

    ICE2A265 PG-DIP-8-6 650V 100kHz 0.9Ω 52W 32W

    ICE2A365 PG-DIP-8-6 650V 100kHz 0.45Ω 67W 45W

    ICE2B0565 PG-DIP-8-6 650V 67kHz 4.7Ω 23W 13W

    ICE2B165 PG-DIP-8-6 650V 67kHz 3.0Ω 31W 18W

    ICE2B265 PG-DIP-8-6 650V 67kHz 0.9Ω 52W 32W

    ICE2B365 PG-DIP-8-6 650V 67kHz 0.45Ω 67W 45W

    ICE2A0565Z PG-DIP-7-1 650V 100kHz 4.7Ω 23W 13W

    ICE2A180Z PG-DIP-7-1 800V 100kHz 3.0Ω 29W 17W

    ICE2A280Z PG-DIP-7-1 800V 100KHz 0.8Ω 50W 31W