This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Original question:
UCC2897A: 输入400V直流,输出30V/7A的有源钳位正激IC推荐
hi.
输入24V,输出5V,输出功率20W,效率>85%
选用UCC2893A是否最合适,如果不是,能推荐更合适的方案吗?
HI
用有缘钳位来做效率是会高一些,可以选择UCC2897A, 可以参考: www.ti.com.cn/.../PMP10871