你好:
BQ76PL455ATPFCTQ1电池断线检测资料中比较模糊,
断线检测设置前后的比较值多少?有没有界定?谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
BQ76PL455ATPFCTQ1电池断线检测资料中比较模糊,
断线检测设置前后的比较值多少?有没有界定?谢谢!!!
您好 ,There is a Squeeze function in BQ76PL455A-Q1 that helps to detect open sense wire conditions. Enabling Squeeze function turns on a 5k Ohm resistor across adjacent VSENSE pins and creates additional voltage drop through the 100 Ohm resistors in series with the VSENSE pins.
This causes an increase in the voltage applied to the window-comparator blocks above and below the inputs that
have the Squeeze resistor applied. To enable the Squeeze function, set TSTCONFIG[EQ_SQUEEZE_EN] =1.
Please refer to BQ76PL455A-Q1 datasheet section 7.3.12.8.1 for more details of an example and block diagram.