This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65185: TPS65185损坏

Part Number: TPS65185


我们的一个电子纸显示屏测试板,使用了TPS65185这个PMIC。上图是我们测试板的TPS65185的外围电路,VIN=4.6V(USB供电5V,串联一个二极管)。

我们的测试板存在一个问题就是TPS65185容易损坏,我们手上已经坏了几十个了,我尝试寻找损坏原因,但是没找到。经我检测,损坏的TPS65185大多数都会出现15PIN-VCOM和PIN8、PIN48-AGND及PIN6-DGND短路的现象。

以上就是我遇到的问题,请帮忙检查一下上面的电路是否存在设计上的问题。还有能不能给出一些建议,让我的测试板避免再出现损坏TPS65185的情况。

非常感谢!