Part Number: UCC2895
UCC2895使用外部19.8KHz的脉冲信号输入到SYNC引脚,窄脉冲信号电平Vin高电平为2.1V,低电平为0V,CT引脚连一个电阻接到RAMP引脚,移相、PWM_ABCD均正常,只是频率不对,不能根据输入的信号的频率设置输出PWM的频率,看手册,SYNC引脚是双向的,只要输入信号频率大于内部振荡器频率,PWM输出引脚就会跟随SYNC输入信号的频率,但经过测试,不能实现,不知道是什么原因,已经被困住1个月了,谢谢解答。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCC2895
UCC2895使用外部19.8KHz的脉冲信号输入到SYNC引脚,窄脉冲信号电平Vin高电平为2.1V,低电平为0V,CT引脚连一个电阻接到RAMP引脚,移相、PWM_ABCD均正常,只是频率不对,不能根据输入的信号的频率设置输出PWM的频率,看手册,SYNC引脚是双向的,只要输入信号频率大于内部振荡器频率,PWM输出引脚就会跟随SYNC输入信号的频率,但经过测试,不能实现,不知道是什么原因,已经被困住1个月了,谢谢解答。
HI
做3个确认?
仅仅SYNC输入,不要RC频率,看是否正常?
不要SYNC输入,仅仅RC频率,看是否正常?
两者都有,SYNC输入30kHz以上,RC仅18.7kHz, 看能否正常?
以上确认主要是怀疑RC频率和SYNC频率太接近导致的异常?