Part Number: TPS74801
HI各位大佬,请问我关于TPS74801我输入3.3V,VBIAS为STBY-5V,输出为2.5V(Iout:1.3A),
1.请问TPS74801可以输出上面的需求吗2.5V,Iout:1.3A?
2.请问VBIAS可以提供一直STBY5V电源吗?还是说这个电源必须和VIN同时一起给?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
可以的, Vbias用5V, Vin 用3.3V, 无需2个输入用同一个电压源。