Part Number: BQ25890
硬件上2 D+和 3D-是拉低的,没有实际的协议输入。
现在遇到问题是,修改完充电电流到2A, 然后Vbus断开,读取reg0B寄存器值是00100111,充电电流是不是被限制到了500mA
有没有办法,在D+ 和D-没有实际协议输入的时候,可以实现充电电流到2A或者3A?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ25890
硬件上2 D+和 3D-是拉低的,没有实际的协议输入。
现在遇到问题是,修改完充电电流到2A, 然后Vbus断开,读取reg0B寄存器值是00100111,充电电流是不是被限制到了500mA
有没有办法,在D+ 和D-没有实际协议输入的时候,可以实现充电电流到2A或者3A?

您好,充电电流,如果D+,D-没有协议,我这里可否修改其它寄存器,比如reg00寄存器,实现调整充电电流大小的限制。
如果我想通过MCU软件控制充电电流大小,有没有指导教程文档。谢谢。
您好,将D+D-短接默认是DCP模式, the digital current limit (IINLIM) to 3.25A.
详细请参考下面链接的内容: