请问TPS61000的效率能够做到85%吗?条件是3~5V输入,5V输出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
TPS61000的输入电压范围为:1.8V~3.3V。如果是3~5V输入,5V输出,建议使用其他IC,比如:LM3488、
LM2700 在输出电流1A的情况下,其效率可达85%。www.national.com/.../LM3488.html

推荐TPS61220: www.ti.com.cn/.../tps61220.pdf
上面有提到TPS61000因为输入输出电压不符而不适合, 按照TPS61000 100mA左右的电流规格,而TPS61220则符合, 在50%~100%的负载范围内效率都可以达到92%左右. 如果要做欠压保护可以通过enable脚,3.3V时Enable分压1.2V, 则1.1V以下芯片必停止工作,或采用其他方法,也可以不用做这个保护,因为芯片自带0.7V的欠压保护。