Part Number: BQ25710
BQ25710适配器供电,要16V以上供电芯片才正常工作,16V以下供电时CHRG_OK引脚为低,且芯片报sys_short故障,请问是什么原因导致?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
Please see attached document.
0552.BQ2570X_BQ2571X_BQ2572X_BQ2573X_SchematicChecklist.pdf
For layout guidance, please see the following FAQ.
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1032723/faq-how-do-i-ensure-the-charger-layout-is-satisfactory-is-there-a-guideline-for-the-buck-boost-charger-controllers-like-bq25713-bq25720-and-bq25730-etc
您好,已经在E2E发帖询问更了解这款芯片的TI工程师,请继续关注。
你好,我看到E2E论坛的工程师有回复问题。具体的细节如下:
1. 如果同时接电池和适配器,VBUS电压范围为7-22V芯片都可以正常工作,电池是3S。如果只是适配器单独供电不接电池,VBUS电压低于16V就会报sys_short故障,发生故障时CHRG_OK为低,Vsys为1.5V。
2. 看到芯片手册说如果移除外部电池要将CELL_BATPRESZ pin拉低,但是我将CELL_BATPRESZ pin做了下拉后芯片就不工作了,会报sys_short故障。
以上是具体的细节描述,麻烦转达。
你好,我看到E2E论坛的工程师有回复问题。具体的细节如下:
1. 如果同时接电池和适配器,VBUS电压范围为7-22V芯片都可以正常工作,电池是3S。如果只是适配器单独供电不接电池,VBUS电压低于16V就会报sys_short故障,发生故障时CHRG_OK为低,Vsys为1.5V。
2. 看到芯片手册说如果移除外部电池要将CELL_BATPRESZ pin拉低,但是我将CELL_BATPRESZ pin做了下拉后芯片就不工作了,会报sys_short故障。
3.该问题是发生在我设计的板卡。
以上是具体的细节描述,麻烦转达。
您好,根据工程师给出的建议,我这边直接跳过前级电路对芯片的VBUS进行供电,用其他信号来打开Q68,并没有解决问题。之前工程师曾经提到过检查VBUS部分的硬件参数,因为芯片故障总发生在固定的VBUS电压范围内,这给了我思路,经过几日的调试,我发现将R595取值改成0Ω后,芯片可以正常工作在4V-24V之间的任意VBUS电压。从目前的情况来看问题应该解决了,非常感谢您的支持!目前主要有以下几个疑问:
1. 将R595取值改成0Ω是否会对芯片的稳定工作产生影响?因为参考设计取值为1Ω;
2.系统正常运行过程中如果移除外部电池要是否要将CELL_BATPRESZ pin拉低?查阅了大多数BQ系列的芯片手册以及评估板模型均有提到该说法。之前有提问过问题,但是工程师还没做出明确的回复;
3,结合第二点请教一下,电池的热插拔场景以及不带电池的工作场景是否为常规操作?是否会影响芯片工作?
目前针对BQ25710的应用主要有以上问题,希望可以解答,非常感谢!