This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS76801使用疑惑



想问一下我的输入是5.5V~7V左右,然后想要一个稳定的5V输出,我的负载大概是1.5W(没有留余量),希望精度在正负2%以内,效率较高的电源芯片,不知道有没有符合这些要求的电源芯片呢,TPS76801可以吗,然后TPS76801的外围电路的电容一定要接低ESR的吗,一般钽电容接上去会有什么影响

  • TPS76801是符合你的要求的,只是如果工作在7V输入的情况下效率会偏低。

    输出的电容要求10uF以上并且ESR在60毫欧到1.5欧姆之间,其原因主要是ESR跟输出电容构成了环路中的一个零点,如果ESR过大会导致这个零点提前从而影响环路的稳定性。至于钽电容是没有问题的,只要满足ESR和容值的要求即可。