This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3845A: 占空比的疑问

Part Number: UC3845A


用TI的工具 WBDesign,自动生成的一个方案

AC = 85.0V---265.0V

Vout = 12.0V Iout = 3.0A

Device = UC3845N  Flyback 

60kHz,CCM

为何设计占空比 才 35.34%,如果选到 45%,不是能减低MOS的电流吗?