This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62866: BUCK 电感计算

Part Number: TPS62866


Hi, TI Support.

请教一个问题,关于BUCK电源的电感值计算。以TPS62866为例计算。

ΔIL=Vo*(1-Vo/Vin) / (L*Fsw) (来自TPS62866 Datasheet P21页,https://www.ti.com.cn/product/zh-cn/TPS62866?keyMatch=TPS62866&tisearch=search-everything&usecase=GPN)

从上式可以得到:L=Vo*(1-Vo/Vin) / (ΔIL*Fsw)。可以看到,电感的纹波电流ΔIL和L成反比,和负载电流没有关系。

ΔIL: 电感纹波电流(p-p值)

Vo:输出电压 3.3V

Vi:输入电压 1.2V

L:电感感值 

Fsw:开关频率 2.4MHz

I:负载平均电流

 

我们一般以ΔIL=(20%~40%)*I 来选择电感感值,取中间值ΔIL=30%*I 。

1、当负载平均电流I=2.3A时,通过上述公式计算出来的电感L=553nH。但webench工具仿真显示,电感只需要取220nH就可以。截图1

2、当负载平均电流I=0.1A时,通过上述公式计算出来的电感L=12.7uH。但webench工具仿真显示,电感仍然只需要取220nH就可以。截图2

 

请问:

1、上述理论计算过程是否正确,如果有误请帮忙指出,谢谢

2、电感值的正确选取方法。是以理论计算结果为准还是以webench结果为准?

3、如果负载电流在一个很宽的范围内变化,电感的取值是否要以最小负载电流来计算(这样会导致电感值很大)