This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A4501的负载要求



想问一下,TPS7A4501的资料上写的输出电压是正负1%的精度,我想问一下这个对负载有要求吗?如果是空载会有影响吗?如果我的输入电压纹波较大,有正负200mv的纹波,输出还能保持这个精度吗

  • Hi Peng liang

    TPS7A4501输出电压是1%的精度是指的直流情况下输出电压的精度。

    当输入电压纹波有200mV时,此时输出应该用PSRR参数来计算

    △Vout=△Vin/[10^(PSRR/20)]

    假设你的纹波频率为1k 那么根据TPS7A4501的datasheet 其PSRR 为68db@1K

    可以求得 △Vout=0.079mV 

    Vout=VoutDC+△Vout

    因此200mV低频纹波是不会影响你精度的。