This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助,bq20z95芯片管理4串55Ah锂电池组中出现的问题



在bq20z95芯片的说明书中,电池组的设计容量可以达到65535mAh,可我实际在使用中Qmax只能设到32767mAh,剩余容量报警也无法设定到10%的设计容量(即5500mAh),提示只能设到700mAh,另设计容量值确实可以设定65535mAh。以上的结果就是初始的满充容量显示为31Ah左右(实际的真实容量为58Ah)。不知如何能解决满充容量显示严重偏低的问题。目前我在对电池组进行小电流充放学习循环,要几天后才能结束。