This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3842炸机问题



最近在调一款12V/2A反激拓扑结构的3842。

输入95-265

输出:12V/2A

工作频率为:80K

变压器的参数为:EF25   原边:辅边:输出边:53:17:10

  L=0.8mH

当我上电的时候,输出正常,也可以工作。问题是:待机功耗很大,自己绕得变压器嚣叫的很。

用示波器看看那个驱动MOS脚 即6脚的波形,看了看,占空比在变,频率也在变。设定是80KHz的。

想是不是IC工作不正常呢?

然后我就去掉VCC的供电部分,直接给IC接一个直流电,此时是慢慢升高电压的,当电压升到16V的时候,IC就炸了,已经炸了几个了,着实心疼。

 

请问这是为什么?