Other Parts Discussed in Thread: TPS5401, TPS54160
最近小弟在做个项目,用到了tps54160与tps5401两款芯片。想问下大家那款更适合做12V到3.3V的降压?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
这两个IC都可以用来做这样的设计,哪个更好,要看你的要求。对这个两个IC做个对比:TPS54160 VS TPS5401
1、输入电压范围:3.5V-60V 3.5V-42V
2、输出电流范围:<1.5A <0.5A
3、效率:两者差不多。
4、控制模式:ECO 模式 电流模式
ECO模式相比于电流模式在环路补偿方面的设计较为简单。
关于DC/DC的选型,可以使用NS的WEBENCH来设计电路。里面可以根据自己的要求选择低成本或高效率或体积小
的。现在TI已将大部分TPS系列的IC整合到这个软件里面。