Hi Team:
我与客户调试TPS65265 芯片时候,发现AUTO 与 External Power Sequencing 模式会有重叠的情况存在,想帮忙确认一下相关的机制与原理,谢谢。
附上实验的数据与问题点:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team:
我与客户调试TPS65265 芯片时候,发现AUTO 与 External Power Sequencing 模式会有重叠的情况存在,想帮忙确认一下相关的机制与原理,谢谢。
附上实验的数据与问题点:
The TPS65265 starts with a predefined power-up and power-down sequence when MODE pin ties HIGH or ties to GND. As shown in Table 2, the sequence is determined by the different combinations of EN1 and EN2 status. EN3 is used to start and stop the converters。
从Excel文档里的描述来看,是不是EN1,EN2,EN3 是同时控制的?如果是的话可以试试分开控制,在EN3=High 之前把MODE, EN1, EN2 的状态按照Table 2 中描述配置好

Hi Sam:
有个疑问是,table 2里面提到auto sequence 里面包含了float 的mode 状态,但是在8.3.5 提到如下图所示的描述,也明确了floating只属于 external control mode。

如下图的参数设定所示,如果都将mode悬空,en1、2都设置成High, 实际输出如何保证是进入auto / external呢?这两个设定都是一致,都符合规格书表中定义,但是输出上电时序可能会有两种,start(BUCK1-3-2)/ start (buck1=2=3), 感觉table2 的auto 时序的float会产生歧义。