This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: 请问如何通过外部输入的方式,把电池温度输入到FuelGauge中?

Part Number: BQ27426

你好,

我们的设备FuelGauge的BIN引脚是接地的,

电池温度需要从外部通过I2C进行输入,OpConfig[TEMPS]配置为10b,这个操作对吗?

配置为10b后,通过Temperature()写入温度(摄氏度转换为0.1k)的操作对吗?

目前的现象:OpConfig [TEMPS]配置为b10,周期写入电池温度的K值,FCCRMSOC都为0

请问如何通过外部输入的方式,把电池温度输入到FuelGauge中?