This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z65 Cell balance设置提问



Min cell deviation是设置内部均衡FET导通的占空比吗?

如果我想设置均衡阈值,可不可以,在哪里设置?谢谢。

  • 因为如果使用内部均衡的话,均衡电流时和外部电阻阻值有关的,所以设置这个数值是告诉电量计多长时间可以均衡出1mAh的电量。占空比典型值是0.4,因为在均衡时电量计隔一段时间还是需要读取电压等数据,所以采用的是固定占空比,通过时间来控制均衡多少,建议这个参数按照实际外围电路和技术手册里进行设置。

    你想设置均衡阈值这个值的是什么条件触发均衡,还是均衡速度?谢谢!