This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510适用4节18650并联吗?



我的设备采用4节18650锂离子电池并联供电,单节2.2Ah,共8.8Ah,电量监测芯片选择的是BQ27510,不知道是否合适?

18650锂离子电池没有温度监测引脚,我也没外接温度传感器,BQ27510的温度引脚我悬空了,不知有无影响。

我已购买EV2300,通讯正常,但电量始终显示100%,进行BQEASY,设置“运行时错误“440”和“6””的错误。

如果这款芯片确实不行的话,可以用哪款芯片代替呢,放电电流在降到3V时差不多有2A。

  • BQ27510适用于一串的锂电池,所有对于4节的锂电池并联应用是合适的。

    TS引脚通过内部电阻和外接NTC电阻分压得到的电压输入到ADC来采集温度。如果电池没有这个引脚的话,可以用来测试系统温度,最好不要悬空。

    关于最后一个问题,请问是怎样核实EV2300的通讯正常的?可否详细描述下《设置“运行时错误“440”和“6””的错误。》这段问题。

  • 并联的方式应该是可以的,但是我的容量有8.8Ah,BQ27510又没说支持多大的容量,所以心里没底。

    EV2300通过USB与电脑连接,与BQ27510通过I2C连接。BQ27510工作正常后,主要是I2C,运行EV2300软件就会显示通讯正常,否则不正常。

    进入软件后,有BQEASY的向导设置,电池容量,节数等,设置完成后,就会开始烧录,烧录的过程中就提示了“运行时错误“440”和“6”,溢出”

  • BQ27510是用于系统端的电量管理芯片.如果是用于pack端,推荐使用BQ27541-V200.

  • BQ27541-G1最高支持32Ah的容量。