设计最大输出电流为20A,带阻性负载时可以达到7A没问题 ,但是带电机时,空载时正常,带负载时约为8A,输出电压由24V降到11V,然后就带不动了,断开负载输出电压恢复到24V,怎么解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
设计最大输出电流为20A,带阻性负载时可以达到7A没问题 ,但是带电机时,空载时正常,带负载时约为8A,输出电压由24V降到11V,然后就带不动了,断开负载输出电压恢复到24V,怎么解决?
Hi
增加大的输出电容,只是有一定的缓解作用。实际上在你的设计中,输出电流9A就已经导致输出电压被拉低,那么带8A的电动机时确实也是会被拉低的。
看起来你的电感饱和电流不够高,原因是按照你说的,你的过电流设计到了26A,但是实际电流输出还没有到这么高,电感已经饱和了,导致输出电压被拉低。
谢谢你的建议,不过我输入电容为两个2200uf并联的,也就是4400uf了。输出电容为1000uf,可能有点小。
我打算把输入电容和输出电容都换成10000uf的大电容。
还有上面的mos管在大电流下很烫,我打算换掉这个mos管试试 。