移动电源电池采用锂电池,需要一路输入,两路输出,输入要能科学的对锂电池进行充电,有充电指示和充满指示,输出5V,分别为1A 、2.1A。最好能有指示灯显示锂电池的电量,请问有没有合适的芯片,望大神推荐一二,小弟不胜感激。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Today, smart phones, PDAs, cameras, etc. can be said that all the necessary digital products, but these are generally not difficult to find the digital product itself is not high capacity, to meet the digital up to people's needs is difficult, the more battery life increasingly short, we need a high-quality power bank, can be a good solution to these problems. For demand, it should be a kind of mobile power need it? Usually they want to move large power capacity, but compact and easy to carry. Simple design and unique personality. Most importantly, the use of safe, all the above are satisfied, is having a very good price.
power bank wholesale,power bank supplier,power bank manufacturer
http://www.qqpowerbank.com/powerbank/