This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596-5V的应用电路怎么设计合理?

Other Parts Discussed in Thread: LM2596

开始设计LM2596-5的电路参考的是TI在线设计电路推荐的电路,如下所示

我的输入是24v,变成5V,然后经过117-3.3变成3.3v,设计的最大输出电流时2.5A,同时用BS0505输出另外一个隔离5V,按照推荐电路设计的,现在随着负载的增大纹波已经接近1v了,一般是400-700mv,太大了,选用的器件也是三洋电容和方形贴片电感,怎么处理呢?求各位大神指导啊,还有手册上推荐电路on/off这个脚是接地的,但是推荐电路没有接地,听谁的?

  • Hi

        在这个电路图的基础上仍建议在输入增加一个330uF~680uF的低ESR电容加强瞬态稳压。

        另外注意输出电容是90mohm,  你可以选择其他的330uF电容,但是一定要注意低ESR。

        关于layout你可以参考一下datasheet。

        上述三点都会影响到输出纹波,做得好正常应该是可以控制在50mV以内的

  • Hi

        见datasheet描述: If this shutdown feature is not needed, the ON/OFF pin can be wired to the ground pin or it can be left open.

        也就是是说保持ON/OFF 接GND或者悬空,都是可以让LM2596正常工作的(On状态),  也因此可以判定芯片内部ON/OFF有下拉到GND.

  • 可以在输出端并联22uf,1uf的陶瓷电容,降低ESR, 同时吸收高频杂波成分,从而降低纹波。