This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

77910A的使用



我想问一下,是不是77910A评估板在常温下一定要提供30V的电源即使用10节电池才能与上位机通信

  • 你好,77910A最低支持4串的应用,不一定要10节才能通信。可以参考user guide 第19 和20页内容。http://www.ti.com/litv/pdf/sluu855

  • 你好我还想问一下,为什么我按照用户手册去测试过压,欠压时,调节独立电源的电压,软件上并不会显示,但是,调节OVT及UVT反而会显示。还有过压和欠压不是针对电池而言的吗,为什么调节电压电池会表现出过压及欠压。

    下面为我的测试方法及结果,求指导

    1)将4节电池接在电池仿真器上(2)在DSG及PACK短接一个电阻,作为负载,CHG端悬空。(3)在CHGCTL及PACK上接一个15k的电阻。(4)在BATT和PACK上接一个32V的独立电源。

    运行过程,首先设置过压相关的寄存器,然后,将电压升高到40V,在下程序,并且读寄存器。结果不会出现过压的状态。而且为什么操作时,只要CHGCTL和PACK一连接就会出现short circuit CHG 断开后又恢复正常。

    还有用户手册上说软件操作时要设置电流的值,我想问一下怎样设置?