大家好,我最近要做一个电源转换的设计,想请大家推荐两款电源芯片!输入信号是12V的开关电源,想获得正负5V的输出。其中+5V输出电流大于2A,-5V输出电流大于1A。由于输出的正负5V将为模拟电路(高速ADC采样电路)供电,所以需要线性电源芯片,以获得比较好的电源性能。请大家帮我推荐一下,谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用LM2588来做, 可以在www.ti.com 里面用webench软件来设计,会有相应的原理图出来
Hi
或者可以用TPS54360+耦合电感来做,参考如下文档:http://www.ti.com.cn/cn/lit/an/slva369a/slva369a.pdf
HI
TPS54360系列(TPS54160/TPS54260等)也可以用来单独做一个-5V, 还有TPS5430,在其官网都是有参考设计的,如:http://www.ti.com.cn/cn/lit/an/slva257a/slva257a.pdf。
但此时就需要两片芯片了。
感谢大家的回复。
由于设计的电源将为高精度的模拟电路供电,用开关电源会不会不太合适。有没有比较好的线性电源芯片推荐下啊!!!
Hi
在DC/DC后面在增加一级LDO, 可以参考:http://www.ti.com.cn/cn/lit/sg/slvt170/slvt170.pdf
(注意前面用到的芯片是TPS54360,采用DC/DC后会大大降低LDO输入输出的压差,降低LDO的功耗)