This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ24195的VBUS和PMID一些疑问

Other Parts Discussed in Thread: BQ24195

Ti的工程师你们好:

        我想用BQ24195做一个移动电源,但是在看规格书的时候发现一个问题:看到框图上VBUS和PMID之间通过一个MOS管相连,BQ24195的输出升压USB输出是接在PMID上的,那么当我的USB设备接在BQ24195的PMID上时,我再在VBUS接入一个12V的电源适配器,此时,无论24195在何种状态,是否工作的情况下,这个12V高压一定会通过这个MOS管的寄生二极管进入我的USB设备,从而导致设备烧坏,但是由于BQ24195是宽电压输入的,BQ24195却不会损坏,是这么理解吗?如果确实是这样,那么这个方案太不安全了,会有至少90%以上发生的概率。