Other Parts Discussed in Thread: LM25088
我在使用LM25088qmh-1产生-12V电源时,发现带负载能力过弱,用水泥负载测试只有300mA左右。然后我通过将R33由10K改为15K(改变工作频率),调整R30和C37分别由200K、330pF改为56K、150pF可以将负载能力增加到500mA左右。但是带负载测试时,带300mA负载,发现电感发热严重,工作一段时间之后不能输出稳定的电压了,请问我的设计有什么问题吗?
电感为sumida的CDRH103RNP-4R7NC-B,可以通过4A电流,30毫欧的内阻。
我的输入电压为12V。