This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24166充电问题咨询

Other Parts Discussed in Thread: BQ24166, BQ24165

用BQ24166对单节锂电池进行充电管理,锂电池容量为8.4Ah,最大充电电流设置为2.5A,原理图如下:

针对原理图,有以下几个问题:

1.系统输出端(电感后端)没有接负载,这样应用是否可以?

2.电池温度监测功能不用的话,TS管脚是否可以悬空?或者怎样连接比较合适?

3.系统设计只用适配器进行充电,那与USB充电功能相关的管脚是否都可以悬空?如果有相关管脚要连接的话,怎样连接比较合适?

4./CE管脚悬空应用是否可以?拉高的话,逻辑电平大概多少合适?

5.该原理图设计有无其它问题?

 

PCB图设计如下图片所示,面积大小为3cmX3cm:

Top面:

 

Bottom面:

 

以上设计的PCB板实际充电时,测试SW管脚的波形如下:

1.不连接电池时,波形如下:

2.连接上电池,充电电流在2A以上时,测得波形如下所示:

现在的问题是,在PCB板Bottem面通过焊锡连接铜箔至地,并且接上散热片,最大充电电流2.5A的时间只能维持半小时左右,然后逐渐下降2A左右才能稳定更长时间(1小时左右),然后充电电流进一步减小, 这样担心电池充不足。如果要使最大充电电流2.5A维持更长时间,有怎样的措施可以实现?或者说这样的原理图和PCB板设计BQ24166工作是否合理?

以上问题请TI专家们详细评估并帮忙解答;

谢谢!

 

 

 

 

 

  • 急用,请TI专家们帮忙解答。

    谢谢!

  • 你好,相关内容基本都可以从datasheet里找到,请阅读规格书里的内容。谢谢!

    1.可以

    2.通过电阻分压使得TS脚电压约为50%VDRV

    3.不能悬空,另外注意RILIM选择。Driving IUSB1, IUSB2, and IUSB3 all high places the bq24165/6/7 in High Impedance mode where the buck converter is shutdown regardless if an input is connected to USB or IN.

    4.拉低Charge Enable Input. CE is used to disable or enable the charge process. A low logic level (0) enables charging and a high logic level (1) disables charging. When charging is disabled, the SYS output remains in regulation, but BAT is disconnected from SYS. Supplement mode is still available if the system load demands cannot be met by the supply. BGATE is high impedance when CE is high