输入10~14VDC,输出-12V/0.1A,非隔离方案请推荐一下芯片。芯片体积要小,效率要高点。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
或者你可以选择TPS54061: 见设计案例:http://www.ti.com.cn/cn/lit/an/slva524/slva524.pdf
12V输入-12V/0.1A输出时效率在85%左右, 不过需要说明的是这款芯片的MOS电流只有250mA(min), 按照12V左右输入,最大输出电流刚好是在0.1A, 同时按照10~14输入,是可以选择小一点的电感以及更低的ESR, 这样效率还将提高。