用LM5007设计一个25V输入,5V输出降压电路,反馈电阻分别选择两个1K电阻,请问一下空载时是否能够稳定输出5V电压?
请求TI专家解答,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用LM5007设计一个25V输入,5V输出降压电路,反馈电阻分别选择两个1K电阻,请问一下空载时是否能够稳定输出5V电压?
请求TI专家解答,谢谢!
Jian Lv1:
您好!LM5007最大输出电流是0.5A,超不了1A啊,但是用示波器实测空载时,Vout端波形为幅度在2-5V之间的一个锯齿波,不是稳定的5V,这是为什么呢?
LM5007在空载时是否可以稳定输出5V呢?
谢谢!
空载输出稳定的5V是完全没有问题的,需要检查下输出电容的ESR,输入电压的最大是多少?工作频率是多少?