This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

下面两个问题请专家帮忙解答下



..

  • 问题1、CHG和DSG是否可以通过手动控制?有没有什么指令或方法,可以关掉bq20z65对CHG和DSG的自动控制,然后直接通过指令手动控制CHG和DSG的开合?

    R :0x46命令是FET控制扩展SBS命令 ,写06可以强制打开充放电mosfet做充放电电气测试。这个命令原本是用于PCB阶段测试电气目的的,不用0x21是因为此时还是一个pcb板,没有贴上cell,如果it enable以后,会影响life time data ,resistence  values update ,以及Qmax的更新。

    测试完了以后要改通过0x46命令将这个控制寄存器复位。

    问题2、bq20z65带有电芯调平衡功能,这个功能是否可以通过指令打开和关闭,例如:当电池处于满电量和空电量之间的任意时候,我想直接通过指令实现对电芯调平衡,可以实现吗?例如:在对电池组充到3.8V时,我就想直接通过指令启动调平衡功能,对4节电芯调平衡,可以做到吗?

    R:电芯平衡功能进行的时间是有讲究的,这样可以避免温度和充电电流以及内阻的影响,按照芯片设计的流程来,否则电芯平衡的精度会受到影响。