This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25118电路不能带负载

根据WEBENCH® Designer上设计的电路进行制版的。上次做过一次,能正常调出结果。这次怎么都不出结果了。

设计范围为6~30V输入,15V/2.5A输出的结构。设计频率为200k,电感值为15uH.Rt选值为27k;

下面说说我遇到的问题吧:

1、空载情况下:

①电路上电后,输出电压上升很慢,大概需要三四秒才能上升到15V。

2、轻载

①先空载启动,当输出稳定后,然后先加3W的负载,输出电压严重跌落,芯片严重发烫;芯片都烧坏了几片貌似。

②带载情况下启动,根本不能启动,没有输出,。

请问,这到底是哪里出问题了????

 

求指导啊。。十万火急。非常谢谢啊。