This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于调试的几个问题,请专家帮忙解答下



我使用的是bq20z65做四节锂电芯的串联检测。调试时遇到下面几个问题,请专家帮忙解答下:

1、我在byeasy里进行5(cycle)的learning时,想把放电电压调低点,应该怎么做?下图的对话框显示放电到12V就不放电了。

2、下图中的电阻RX是官方电路上的哪个电阻?V_avg指的是哪个SBS中的哪个量?

3、是不是充放电都可以电芯平衡?还是当有电芯充满了,才对其它电芯执行电芯平衡?可以设置电芯平衡的电压点吗?例如在3.6V以上开始执行电芯平衡。