请教:
1. 为BQ2050H供电时,DATASHEET上面说VCC额定的最大值为6.5V,我用两节锂电池电压7.2V,直接接上VCC一定会超过这个值。找到了一篇TI上的应用,如上图,图中红线框住的部分上VCC与电池BT+之间加的是MOS管2N7002,它的导通电压Vgs=2V左右,而mos管的栅极接的是BQ2050的REF管脚。请问这部分电路是如何运作的?
2. 电路中有很多BAV99的管子,图中红线画出来的部分,请问它一般起什么作用的?
谢谢各位
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.这部分的电路类似于一个LDO作用,
2.应该是起到ESD保护作用,
同时如果是两串锂电池应用,推荐使用BQ28400,因为BQ2050H是一个比较老的型号,