我使用BQ34Z100对16节串联电池单体进行监测,在的过程中,请问一下:
(1)如何确定Ra Table的一系列值呢?16节电池对应的15个Ra值应当怎么测量?
(2)SOC的值是否一定要充电放电学习后才能测准呢?学习时是否要从0%到100%来回进行测试?(因为每次芯片断电重新上电后,SOC的值都变成了0)。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用BQ34Z100对16节串联电池单体进行监测,在的过程中,请问一下:
(1)如何确定Ra Table的一系列值呢?16节电池对应的15个Ra值应当怎么测量?
(2)SOC的值是否一定要充电放电学习后才能测准呢?学习时是否要从0%到100%来回进行测试?(因为每次芯片断电重新上电后,SOC的值都变成了0)。
谢谢。
(1)这个数值是在golden learning过程中 电量计自行学习更新得到的
整个过程需要完成:参数配置,CHEM-ID选择,校准,然后才能进行golden learning,golden learning必须满足一定的充放电条件。BQ34Z100的基本过程和单节时类似的,除了多了与多节相关的几个参数
可以先参考这个帖子:http://www.deyisupport.com/question_answer/analog/battery_management/f/35/t/46539.aspx
(2)不需要,确认下是否使能了IT算法,实际量产只需要使用golden file即可达到一个比较好的精度,如果可能的话请附上GG和log文件,谢谢!
我测试了一下,在配置好dataflash之后,进行标定时,按照标定界面的顺序,在进行电流标定时,我使用恒流6A对电池组进行充电时,发现这时标定界面上的“Measureed Voltage” "Measureed Temperature"以及“Measured Current”这些值都在跳变,有正有负,点击“Calibrate PACK Current”时,会出现“error reading DF CAL value” 或者”error setting to GG mode “ 请问这是什么原因?谢谢