This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65912: EN信号使能后输出无设定上电斜率(slew rate)

Part Number: TPS65912


如上图,为使用需求, 目前希望通过ENx 引脚 分别控制三路DCDC的上电、下电。

目前遇到的问题是,配置好寄存器,EN信号开启和关闭后,电源输出能够按照EN信号响应开关,但是无斜率呈现(上下电斜率无法调节)。

使用目前config1=0 config2=1 使用的op reg,    DCDC1_CTRL (00h) =0x1C  DCDC1_AVS (05h) =0xb8    DCDC1_OP (04h)=0x38  DCDC1_LIMIT (06h) =0xFF  EN1_SET2 (30h)=0x04

IO_PMU_CONFIG2,FUNC=GPIO_PV_HIGH
IO_PMU_CONFIG1=GPIO_PV_LOW
IO_PMU_PWRHOLD_PIN=GPIO_PV_HIGH
IO_PMU_SLEEP_PIN=GPIO_PV_HIGH
IO_PMU_nPWRON=GPIO_PV_LOW

通过调节DCDC1_OP (04h)=0x38  DCDC1_OP (04h)=0x00 可以控制电源的斜率电压上下电(根据寄存器CTRL(00)可控斜率),但因为00对应电压有0.5V ,需求是从0V 上下电。(如上图所示)

想请问设置好寄存器后, EN信号本就不支持 开启带斜率输出,还是我的配置上(IO信号或者寄存器)需要调整呢 ?

as the picture shown above,I need  controlling three DCDCs output by ENx Signal, but after setting reg CTRL00、OP04、AVS05,LIMIT06, EN1_SET2 (30h).  By changing EN pin level, It can't output voltage with aim slew rate,  while change reg[04] is useful to output voltage while slew rate , but it can't power on or power off from 0V(the least voltage 0.5V as spec defined )

Can EN signal control output voltage with slew rate?