This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

锂电池电量监测方案咨询



现在使用3节锂电池串联起来做成一个电池包,电池电压12V以上,容量在2.4Ah,对外只有Pack+,Pack-两个引脚,能否使用BQ27425,BQ27421来进行电量监测?

如果不行,TI专家帮忙推荐一款好的方案。

谢谢!

  • 你好,锂电池串联很关键的一点是保护和均衡功能,所以如果可能的话尽量在电池包里面使用TI的2-4节电量计,比如BQ20系列和BQ30系列。如果精度要求不高并且电芯一致好的话,是可以考虑使用单节的电量计分压进行计算,但是BQ274系列的电量计BAT,REGIN等管脚的输入电压范围小,如果用的话还需要外加一个LDO。考虑一个均衡保护IC+LDO+BQ274XX综合成本,还是建议使用多节电量计方案。

  • 你好 BQ274系列的电量计BAT,REGIN的这两个引脚 不是测量电池电量的吗   如果加上 LDO 还能测量电池的电量吗   新手请多多包涵