This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps2384无有效输出

Other Parts Discussed in Thread: TPS2384

参考了ti的demo,利用tps2384设计的4口pse,设置如下:

1,ms拉低(自动模式);

2,wd_dis拉低,alta/b拉高;porb拉高;

3,48v输入,利用网口45做正极,78做负极;

实测如下:

空载时,3.3v和10v正常,6.3v实测5.1v,intb实测2.2v;

负载时,3.3v和10v正常,6.3v实测5.9v,intb实测1.7v;

数字万用表实测p始终48v,n则在45.2-17-33.1-37.7-27.8等跳变。pn的示波器波形几乎无规律。

求助:目前是什么状态?哪里出错了么?请大神帮助解答,谢谢。

  • 从N端的电压来看,有可能是握手不匹配,PSE端在不断检测. 请检查PD端的DEN和CLASS等PIN脚设置是否正确? TPS2384只能匹配供电802.3af的PD,另外请把你的PSE和PD端电路原理图发上来看一下.

  •  不好意思,上周出差在外,没能及时查收邮件。
        附件为我们的pse端的原理图,需要注意的是,光耦部分都已经nc了,因为我们希望2384工作在auto mode下。
        暂时拿不到pd端的原理图。
        还请先就这pse端设计,帮我们查看一下原因。如果需要在硬件上调试,来判定问题所在时,请尽快通知联系我们(ants_hw@163.com),谢谢。
    SCHEMATIC1 _ PAGE1.pdf
  • 你好,PSE端电路原理图我看了一下基本上是按照我们评估板来设计的,PSE端是通过RJ45接口的45,78来传输电源,检查对应的PD端是否也是45,78来接收电源 ?

    另外我们会线下联系你,谢谢.