請問各位我在做一個3S2P的Battery Pack,LED有4顆顯示電量,目前充到第4顆LED閃爍時發現第二顆也會一起閃
想請教一下為何會有這個現象呢...(PF Error code 我也設定成00了)
謝謝各位
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
請問各位我在做一個3S2P的Battery Pack,LED有4顆顯示電量,目前充到第4顆LED閃爍時發現第二顆也會一起閃
想請教一下為何會有這個現象呢...(PF Error code 我也設定成00了)
謝謝各位
您好,
the LED chg thresh 5 must be set to 101%. You will not be able to do this with the bqz so it would have to be done manually with a DF write using the advanced comm tab.
here's how to change it to 101%:

Do a write block with 0x44 as command and the data in the image in the block.