Part Number: BQ40Z50-R1
請問各位我在做一個3S2P的Battery Pack,LED有4顆顯示電量,目前充到第4顆LED閃爍時發現第二顆也會一起閃
想請教一下為何會有這個現象呢...(PF Error code 我也設定成00了)
謝謝各位
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ40Z50-R1
請問各位我在做一個3S2P的Battery Pack,LED有4顆顯示電量,目前充到第4顆LED閃爍時發現第二顆也會一起閃
想請教一下為何會有這個現象呢...(PF Error code 我也設定成00了)
謝謝各位
您好,
the LED chg thresh 5 must be set to 101%. You will not be able to do this with the bqz so it would have to be done manually with a DF write using the advanced comm tab.
here's how to change it to 101%:

Do a write block with 0x44 as command and the data in the image in the block.