断开Lvio 和 Cvio.out后, 测量Lvio与Cvio.out的连接点电压,还是2.3V
请问是什么原因造成了这个问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Zhixin Zhao 说:Osial 您好,请问io_1p8_in的是什么作用?如果不考虑io_1p8_in的影响,vio_out的输出应该是多少呢?我怀疑是LC电路没有起到降压的作用,不知道我的怀疑是否有道理。如果只用dc-dc输出,是不是io_1p8_in没有作用,它是不是只是一个输入引脚。
io_1p8_in是一个输入引脚,供电给IO口,我的担心是这个输入引脚影响了DCDC的输出。
LC你选择推荐的1uH, 10uF应该就没有问题。Debug的思路应该是断开VIO和后面的所有连接,看看是否问题解决了。
这路电压的输出为1.8V或者1.85V,具体请参考Datasheet(http://www.ti.com/lit/gpn/tps65950)41页的表格。
Zhixin Zhao 说:io_1p8_in与vio_out是电路板内部连线,割线的方式断开后端就破坏了电路板。VIO DC-DC是一个独立的开关电源,在有电源输入的情况下自己应该不受其他引脚功能的影响吧?LC电路起到在MOS管关闭时的电源的持续性,同时VIO_OUT是不是反馈引脚,不能主动输出?
还有如果是io_1p8_in引脚引起的问题,会有什么原因引起的呢,如果不破坏电路板的话,我可从其他方面排查问题
有一个脚脚VIO.FB应该是反馈脚。
看一下SW的波形,看是否是最大占空比了?如果是的话,有可能反馈脚虚焊了,导致环路没有正常工作。