This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92641: 大电流LED恒流电源驱动方案推荐

Part Number: TPS92641


各位工程师好

我有个机器视觉方案要用LED照明方案,具体需求如下:

恒流控制。

输入电压: 24 or 48V  二选一,可以根据驱动芯片来定

输出:一组(多组) led灯珠串联(并联)  额定工作电压在 24~48 V之间,输出电流0.5A ~ 5A(0.5A~3A)。

输出控制方式: 脉冲(单脉冲)触发点亮,点亮时间长度10ns~1us(50ns-1us),从点亮到电流稳定时间在10ns以内为佳。

感谢各位能提出方案和意见。