请教,之前使用一个sample进行了golden learning,update status为06,将senc文件导出,并写入新的电池包中,发现FC值为800,而golden sample的FC值为24000,究竟什么原因导致,新的电池包是否还需做一轮充电、搁置、放电等学习过程?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教,之前使用一个sample进行了golden learning,update status为06,将senc文件导出,并写入新的电池包中,发现FC值为800,而golden sample的FC值为24000,究竟什么原因导致,新的电池包是否还需做一轮充电、搁置、放电等学习过程?
重新选择了chemistry_ID(同一厂家的电芯,都是储能型的,只是容量相差100mAh),在学习过程中发现三个问题:1、放电时,当SOC为31%时,一直保持不变,直到放电达到截止电压,SOC一下变为0%;2、BQ34Z100中cell Terminate Voltage设置低限值为2.5V,而规格书上放电终止电压为2.0V;3、学习后Up_status始终为05; 附件为学习是log数据,请帮助分析一下,谢谢!
电池材料是那种类型,建议选择一个电芯做chem ID-select
1.能否提供gg文件,如果chem-ID golden learning以及参数设置都正确发生这种现象确实比较异常
2.一般锂电池2.0V-2.5V之间的电量并不是太多,所以设置2.5V即可
3.这种情况的可能原因有一种是chem-ID没有选对,所以建议重新选择ID 然后重新做golden learning
John,
1.这个问题原因和解决方式如另外一个帖子里我所回复的http://www.deyisupport.com/question_answer/analog/battery_management/f/35/t/52097.aspx