Dear Engineer:
- There is a question about TPS54386 buck IC I want to seek your help.
Referring to your IC's Datasheet,under the classic configuration of this IC(24V to 5V/12V),our company found a question that output will be reopened before and after the IC is powered on,as shown in the following waveform:
Power on | Power off |
- After a series of tests and verification,it is found that the configuration of the IC peripheral circuit has no effect on this re-opening mis-triggering phenomenon,so it is verfied that the FB output pin will mis-trigger the output voltage (as shown in waveform in the table below) when the TPS54386 IC input about 7V voltage to its PVDD pin.I look foward to the active cooperation of engineers based on the analysis of solutions.Looking forward to your reply,thank you.
Power on(6~8Vlotage of PVDD) |