近期项目使用UCC27523驱动推挽电路,信号源使用的DDS输出的互补PWM波,占空比无法调节,为50%.
实际驱动时,发现两路MOS管输出有交叠,导致电源毛刺非常大,且器件发热。
请问有什么方法加入死区或者其他什么吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCC27523是不带死区的驱动器,你需要互补输出的话可以只用一路,然后加一级反向器,一般反向器芯片里面都有多个非门,用一个时间延时不够可以用三个。如果你想做可调的死区时间,可以另外添加死区时间电路。
Hi,
可以尝试在UCC27523的输入端加RCD电路,目的是使驱动输入的上升沿通过RC充电上升慢,而下降沿通过D放电速度快,来制造死区。
如果UCC27523的阈值为TTL触发,可能制造的死区不够。可以尝试用CMOS触发的驱动,比如说UCC27528,其开通关断阈值为VDD的百分比。
Regards