This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在 Webench Power design输入需求,推荐的技术方案是UCC256303+UCC24624,在TI的官网下载仿真模型,只有SIMPLIS Model,分别下载这两个IC的model,在SIMPLIS仿真软件下面,可以正常运行,没有报错,并有正常输出结果。
参照 Webench Power design推荐电路,以UCC256303(SLUM601.ZIP)为基础,将UCC24624电路(SLUM645A.ZIP)复制到新电路中,仿真报错,信息如下:
<<<<<<<< Error Message ID: 1023 >>>>>>>>
input file /UCC256303+UCC24624/SIMPLIS_Data/UCC256303+UCC24624 01.deck, line 131:
X$U1 67 74 0 88 77 93 85 75 UCC24624RTM
Unable to locate the definition
of 'subcircuit UCC24624RTM' in the input, include, or library file(s).
On SIMetrix/SIMPLIS Elite with Verilog for SIMPLIS - Magnetics Design Module - DVM, Version : 8.40
*** END SIMPLIS ERROR REPORT ***
请帮忙解决问题,谢谢!
Hi
以UCC256303(SLUM601.ZIP)为基础,将UCC24624电路(SLUM645A.ZIP)复制到新电路中,仿真报错。 用的是什么软件?