在I2C Pro界面中,
1、BQ27541怎么设置和使用?
2、该界面是干嘛用的?
3、在Write I2C Data Block中,Data Block左边方框中输入000F,然后点击左边的Write Data,更新后EVSW无法与电池通讯了,板子报废了?怎么恢复正常?
顺便问下,有没TI电量计的Q群呀?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在I2C Pro界面中,
1、BQ27541怎么设置和使用?
2、该界面是干嘛用的?
3、在Write I2C Data Block中,Data Block左边方框中输入000F,然后点击左边的Write Data,更新后EVSW无法与电池通讯了,板子报废了?怎么恢复正常?
顺便问下,有没TI电量计的Q群呀?
1.第一次使用可以先参考这个帖子http://www.deyisupport.com/question_answer/analog/battery_management/f/35/t/46539.aspx
2.这个界面是I2C操作电量计,同时主要是读写senc文件,senc文件包含电量计所有软件信息,包括所有参数和firmware
3.这个是进入ROM模式,TI单节电量计常见有2中模式,不同模式I2C地址不一样,一种是firmware模式也就是正常运行的模式(地址AA),一种是ROM模式(地址16),ROM模式下可以用于烧写senc文件,你点下面的执行按键就可以恢复,或者电量计掉电重启
谢谢
还有一个问题——在I2C窗口中,为什么点击Program或Read to *senc file会弹出"Comm error code=772"的错误信息?
请问bq27541的FAS和SS被锁住了,如何解锁呢?
我在control 不小心输入了0020
现在进不到ROM模式了
可以试一下默认的key看能够解锁。在这个界面确保没有扫描和log数据,然后control里输入0414 回车 3672回车 FFFF回车 FFFF回车,
如果可以解锁进入ROM重新刷一个没有加锁的senc就恢复 了
你好,知道chem id后,怎么设置到芯片里面去,会有对应的文件吗?然后把文件导进去?